Dual STUSB4710 Power Management
I am designing a usb type-c charger.
I want to use 2 microcontroller and 2 STUSB4710.
Type-C Output will be 20V 3.35A 67W.
I want to do power management between these USB Type-C outputs.
I have questions. Can you please answer them?
1. Are there any I2C command to close the output pmosfets with STUSB4710?
2. Can microcontroller reduce the output current capabilities of STUSB4710 while a device connected to USB Type-C sinking some current. For example,
- Default output contract is 20V 2.25A
- Send I2C command to STUSB4710 and change the output capabilities to 20V 3A.
- Output contract is now 20V 3A.
- Attach a usb device which sinking 20V 3A power and start consume 60W.
- Send I2C command to STUSB4710 and change the output capabilities to 9V 2.25A.
- STUSB4710 send message over CC communications.
- Sink device reduce power consumption to 9V 2.25A.
- Is the scenario possible? If there is a problem, can you correct it?
3. Is there any other way to reduce sinking current of the connected usb device?
4. STUSB4710 supports 20V 5A. But Vconn is not supported with STUSB4710. Is there a standard incompatibility?
5. Is 20V 3.35A type-C output possible with STUSB4710?
6. I have found this post https://community.st.com/t5/interface-and-connectivity-ics/stusb4700-4710-i2c-register-details/td-p/234334. But I did not find any clear guidelines(step by step) for changing register and effects of it. Also some registers contained TBD values.