Elaborate correct number for max_attr_records in aci_gatt_add_serv
I'm struggling to get some detailed information on how to determine the correct number for the max_attr_records value of the aci_gatt_add_serv() function.
I know that you need 1 for the service itself and then at least 2 for each characteristic, but what else requires an attribute record?
Let say I have the following characteristic
aci_gatt_add_char(hServiceConfiguration, UUID_TYPE_128, uuid, 6,
CHAR_PROP_NOTIFY|CHAR_PROP_READ|CHAR_PROP_WRITE, ATTR_PERMISSION_ENCRY_WRITE,
GATT_NOTIFY_READ_REQ_AND_WAIT_FOR_APPL_RESP,
16, 0 , &hCharTripConf);
What would be the resulting number of attribute records? I came up with 4, but I'm not sure if that's correct.
Further, there seems to be a limit for the total attribute records as I can only add a quite limited amount of services. How is this limit defined?