Skip to main content
Associate III
November 1, 2024
Question

Error "Failed to create cookie file 'h:/.erlang.cookie'" installing lorawan-server

  • November 1, 2024
  • 3 replies
  • 1079 views

Hi,

I am trying to install a Lorawan network server on a local computer following the instructions provided here: How to create a LoRaWAN server on local PC (1/2) - STMicroelectronics Community

I am installing it on a Window 10 machine, and had an error " format: "Failed to create cookie file 'h:/.erlang.cookie': enoent" when ran lorawan-server.bat in Windows command line console (as an administrator). Just wondering if anyone had same experience and how to fix it? 

Thanks,

Olive

3 replies

Andrew Neil
Super User
November 1, 2024

Note that the server is a 3rd-party open-source project - not an ST product:

AndrewNeil_1-1730470692173.png

So that would be the place to get support for it:

AndrewNeil_2-1730470756793.png

https://github.com/gotthardp/lorawan-server

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
OliveAuthor
Associate III
November 1, 2024

Thanks for the reply! I will try lorwan server support then.

-Olive

OliveAuthor
Associate III
November 1, 2024

Addition to the information I posted above, I don't have a hard drive named "h" on my PC. I have no idea which file is requiring it and where to modify it.

-Olive

OliveAuthor
Associate III
November 11, 2024

Just would like to give a follow-up regarding the above issue: The lorawan server was installed successfully on an old Windows 7 PC without any issue following the instructions provided in the post: How to create a LoRaWAN server on local PC (1/2) - STMicroelectronics Community

I was not able to install the application server as the node-red does not support Windows 7.

-Olive