hci_reset function returns BLE_STATUS_TIMEOUT with BLUENRG-M2SA in network co-processor mode
I have BLUENRG-M2SA BLE module that I am trying to interface with STM32l496 IC.
I generated the code through STM32CubeMX using X-CUBE-BLE2 v3.3.0 selecting HCL_TL Basic and HCL_TL_INTERFACE UserBoard.
The code gets compiled and when I try to flash and debug, hci_reset function returns BLE_STATUS_TIMEOUT error.
Following are connections
STM32 BLUENRGM2SA
SPI_MISO DIO2
SPI_MOSI DIO3
SPI_CLK DIO0
GPIO_OUT DIO11 // CS
GPIO_OUT RESETI read DT0137 Design tip manual to make the following changes when using BLUENRG-M2SA development board:
HS_SPEED_XTAL=HS_SPEED_XTAL_32MHZ
LS_SOURCE=LS_SOURCE_EXTERNAL_32KHZ
SMPS_INDUCTOR=SMPS_INDUCTOR_10uH
The macros seems to be renamed as following:
HS_SPEED_XTAL=HS_CRYSTAL_32MHZ
LS_SOURCE=LS_SOURCE_32KHZ
SMPS_INDUCTOR=SMSP_10uH
Above changes were made but still it throws the same error.
Do we need to make any additional changes to use BLUENRG-M2SA in a network co-processor mode? I directly opened the packing, soldered on custom board and using it.
What could be the reason for this issue and how to resolve this issue?