Skip to main content
LMyle.1
Associate III
October 18, 2022
Question

Hello I am interested in an ST-Link cable connector which requires the least amount of pins from a JTAG connector can you please reccomend something please ?

  • October 18, 2022
  • 1 reply
  • 1201 views

..

This topic has been closed for replies.

1 reply

Technical Moderator
October 20, 2022

For ST-LINK V2, JTAG cable is used for connection to a standard JTAG 20-pin pitch 2.54 mm connector, and for ST-LINK-V3, Flat cables STDC14 to MIPI10 / STDC14 / MIPI20 (connectors with 1.27 mm pitch)

You can refer to AN4989 for more details

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL