Hello, I am using libraries available from ST for developing applications based on S2-LP module. I would like to be able to reach a communication distance between 2 devices that is at least 1 KM. I am attaching my current radio configuration. BR
/* Defines ---------------------------------------------------------------*/
#define XTAL_OFFSET_PPM 0
#define INFINITE_TIMEOUT 0.0
#define BASE_FREQUENCY 868.0e6
#define CHANNEL_SPACE 100e3
#define CHANNEL_NUMBER 0
#define DATARATE 38400
#define FREQ_DEVIATION 20e3
#define BANDWIDTH 100E3
#define POWER_INDEX 7
#define RECEIVE_TIMEOUT 2000.0 /*change the value for required timeout period*/
#define RSSI_THRESHOLD -120 /* Default RSSI at reception, more
than noise floor */
#define CSMA_RSSI_THRESHOLD -90 /* Higher RSSI to Transmit.
If it's lower, the Channel will be seen as busy */
/* Packet configuration parameters */
#define SYNC_WORD 0x88888888
#define LENGTH_WIDTH 7
#define CRC_MODE PKT_CRC_MODE_8BITS
#define EN_FEC S_DISABLE
#define EN_WHITENING S_ENABLE
#define MODULATION_SELECT MOD_2FSK
#define POWER_DBM 16.0
#define PREAMBLE_LENGTH PREAMBLE_BYTE(4)
#define SYNC_LENGTH SYNC_BYTE(4)
#define CONTROL_LENGTH 0x00 //PKT_CONTROL_LENGTH_0BYTES
#define VARIABLE_LENGTH S_ENABLE
#define EXTENDED_LENGTH_FIELD S_DISABLE
#define PREAMBLE_BYTE(v) (4*v)
#define SYNC_BYTE(v) (8*v)
#define VARIABLE_LENGTH S_ENABLE
#ifndef USE_BASIC_PROTOCOL_ADDRESS
/* Addresses configuration parameters */
#define EN_ADDRESS S_DISABLE
#define EN_FILT_MY_ADDRESS S_DISABLE
#define EN_FILT_MULTICAST_ADDRESS S_DISABLE
#define EN_FILT_BROADCAST_ADDRESS S_DISABLE
#define EN_FILT_SOURCE_ADDRESS S_DISABLE//S_ENABLE
#define SOURCE_ADDR_MASK 0xf0
#define SOURCE_ADDR_REF 0x37
#define MULTICAST_ADDRESS 0xEE
#define BROADCAST_ADDRESS 0xFF
#else
#define EN_ADDRESS S_ENABLE
#define EN_FILT_MY_ADDRESS S_ENABLE
#define EN_FILT_MULTICAST_ADDRESS S_ENABLE
#define EN_FILT_BROADCAST_ADDRESS S_ENABLE
#define EN_FILT_SOURCE_ADDRESS S_ENABLE
#define SOURCE_ADDR_MASK 0xf0
#define SOURCE_ADDR_REF 0x37
#define MULTICAST_ADDRESS 0xEE
#define BROADCAST_ADDRESS 0xFF
#endif
#define EN_AUTOACK S_DISABLE
#define EN_PIGGYBACKING S_DISABLE
#define MAX_RETRANSMISSIONS PKT_DISABLE_RETX
#define PAYLOAD_LEN 25 /*20 bytes data + tag + cmd_type + cmd + cmdlen + datalen*/
#define APPLI_CMD 0x11
#define NWK_CMD 0x22
#define LED_TOGGLE 0xff
#define ACK_OK 0x01
#define MAX_BUFFER_LEN 96
#define TIME_TO_EXIT_RX 3000
#define DELAY_RX_LED_TOGGLE 100
#define DELAY_TX_LED_GLOW 100
#define LPM_WAKEUP_TIME 100
#define DATA_SEND_TIME 50