Skip to main content
TYang.5
Visitor II
January 29, 2021
Question

Hi. Can anyone tell me how to BlueNRG-X_Flasher_GUI.exe to program the target chip? Command Line Download Fireware......

  • January 29, 2021
  • 0 replies
  • 514 views

Dear ALL,

I can use BlueNRG-X_Flasher_GUI.exe to program the target chip,please see attached picture 1

0693W000007CyF3QAK.png 

But I want to use BlueNRG-X_Flasher_Launcher.exe to download, but I can’t do it. Here

is my attempt to follow the Commands.

Below is the command I tried:

C:\Users\TenoYang>BlueNRG-X_Flasher_Launcher.exe flash -SWD -all -f "C:\STLink.b

in"

Working on ST LINK:

 1)\ (x)

09:15:16.542:

STLink A -> Waiting device to flash...09:15:16.598:

STLink A -> Waiting device to flash...09:15:16.653:

STLink A -> Waiting device to flash...09:15:16.743:

STLink A -> Waiting device to flash...09:15:16.795:

STLink A -> Waiting device to flash...09:15:16.846:

STLink A -> Waiting device to flash...09:15:16.897:

STLink A -> Waiting device to flash...09:15:16.947:

STLink A -> Waiting device to flash...09:15:16.996:

STLink A -> Waiting device to flash...09:15:17.052:

STLink A -> Waiting device to flash...09:15:17.098:

STLink A -> Device to flash not connected.

****

INPUT PARAMETERS FOR FLASH OPERATION****

-

OPERATING MODE = SWD

-

CMSISDAP = DISABLE

-

FREQUENCY = 4000

-

BLUENRG-1 DEVICE FILE = C:\STLink.bin

-

BLUENRG-2 DEVICE FILE = C:\STLink.bin

-

BLUENRG-LP DEVICE FILE = C:\STLink.bin

- VERIFY

= False

- MASS

ERASE = False

- START

ADDRESS = 0x10040000 (only for .bin image file)

- READOUT

PROTECTION = False

- MAC

ADDRESS OPTION = False

- LOG =

False

****

RESULTS OF FLASH OPERATION ***

1 -

Device connected with STLink A (\x34\x3f\x6c\x06\x41\x55\x30\x39\x43\x16\x21

\x57)

Device =

None

Command

-> FLASH = Fail

WARNING

MESSAGE:

Device to

flash not connected.

Q:How to use BlueNRG-X_Flasher_Launcher.exe to download a bin file to the target chip

(BlueNRG-LP QFN48)???

Why doesit prompt that the device cannot be connected? Is my commands not correct?

could you give me some advice.

Looking forward to your reply, thank you very much!!

This topic has been closed for replies.