Hi I am implementing a nrf24l01 driver with the use of stm32F4 the SPI transmit and receive works with the polling method yet not with DMA method.I already configured the DMA on cube mx and IAR WORKBENCH this is the code part i put the dma as cmnt
//3. Read single byte from a register
uint8_t NRF24_read_register(uint8_t reg)
{
uint8_t spiBuf[3];
uint8_t retData;
//Put CSN low
NRF24_csn(0);
//Transmit register address
spiBuf[0] = reg&0x1F;
HAL_SPI_Transmit(&nrf24_hspi, spiBuf, 1, 100);
// HAL_SPI_Transmi_DMA(&nrf24_hspi, spiBuf, 1);
//Receive data
HAL_SPI_Receive(&nrf24_hspi, &spiBuf[1], 1, 100);
// HAL_SPI_Receive_DMA(&nrf24_hspi, &spiBuf[1], 1);
retData = spiBuf[1];
//Bring CSN high
NRF24_csn(1);
return retData;
}
//4. Read multiple bytes register
void NRF24_read_registerN(uint8_t reg, uint8_t *buf, uint8_t len)
{
uint8_t spiBuf[3];
//Put CSN low
NRF24_csn(0);
//Transmit register address
spiBuf[0] = reg&0x1F;
//spiStatus = NRF24_SPI_Write(spiBuf, 1);
HAL_SPI_Transmit(&nrf24_hspi, spiBuf, 1, 100);
// HAL_SPI_Transmi_DMA(&nrf24_hspi, spiBuf, 1);
//Receive data
HAL_SPI_Receive(&nrf24_hspi, buf, len, 100);
HAL_SPI_Receive_DMA(&nrf24_hspi, buf, len);
//Bring CSN high
NRF24_csn(1);
}
//5. Write single byte register
void NRF24_write_register(uint8_t reg, uint8_t value)
{
uint8_t spiBuf[3];
//Put CSN low
NRF24_csn(0);
//Transmit register address and data
spiBuf[0] = reg|0x20;
spiBuf[1] = value;
HAL_SPI_Transmit(&nrf24_hspi, spiBuf, 2, 100);
//HAL_SPI_Transmit_DMA(&nrf24_hspi, spiBuf, 2);
//Bring CSN high
NRF24_csn(1);
}
//6. Write multipl bytes register
void NRF24_write_registerN(uint8_t reg, const uint8_t* buf, uint8_t len)
{
uint8_t spiBuf[3];
//Put CSN low
NRF24_csn(0);
//Transmit register address and data
spiBuf[0] = reg|0x20;
HAL_SPI_Transmit(&nrf24_hspi, spiBuf, 1, 100);
//HAL_SPI_Transmit_DMA(&nrf24_hspi, spiBuf, 1);
HAL_SPI_Transmit(&nrf24_hspi, (uint8_t*)buf, len, 100);
//HAL_SPI_Transmit_DMA(&nrf24_hspi, (uint8_t*)buf, len);
//Bring CSN high
NRF24_csn(1);
}