High current draw on BlueNRG-LP STEVAL-IDB011V1
Hello,
I'm doing some development work with an STEVAL-IDB011V1 dev board. I'm targeting very low power and so I would like to verify the numbers listed in the datasheet.
In DEEPSTOP mode at room temperature, I am expecting something around1 μA of supply current, per table 24 of the BlueNRG-LP datasheet. However, I'm currently measuring about 5.7 μA at 1.8 V.
I'd like to make sure my methodology in measuring this is correct. My procedure is as follows:
I flash the board with code that runs SystemInit(), configures all GPIOs to have a pulldown resistor and to output low, and then enter DEEPSTOP. I then unplug the board and remove all jumpers (JP1 - JP5). I connect the positive terminal of my 1.8 V power supply to pin 2 of JP1 (named "VBLUE" in the STEVAL-IDB011V1 data brief) and the negative terminal to ground.
I get a somewhat steady 5.7 μA of supply current from my power supply. I also tried connecting VBRD to ground, which changes my supply current to 13.8 μA. I'm not running any timers, so from the datasheet, I'm expecting 0.65 μA.
I'm hoping someone has some advice regarding my methodology or any input as to why my current is as high as it is.
Thanks for the help.