How do I interpret the maximum Output voltage Vo on the STP16CPC26
I want to connect 7 LED's on one output in series, using a current of 20 mA. Each LED can have a forward voltage of 3V, which means 7 x 3 = 21 V. I want to use a power supply of 24V.
I read in the specifications that the max Vo (Output Voltage) is rated 20V. But how do I interpret this? If I drive my LED's, each taking 3V, the voltage on the output pin will only be 24V - (7 x 3V) = 3V, which is far below the max rated Output Votage.
With other words, powering my LED's with a 24 V power rail is not a problem?