Skip to main content
ffwali
Visitor II
September 29, 2022
Question

How to add and switch between multiple eSIM profiles in ST4SIM200?

  • September 29, 2022
  • 1 reply
  • 2674 views

I have B-L462E-CELL1 development board with ST4SIM200M IC. this board came pre-provisioned with the Truphone profile but I didn't find any way to add a new profile. According to the datasheet eSIm chip supports up to 7 profiles but How can we add and switch between different profiles?

    1 reply

    Visitor II
    January 21, 2025

    I also have same question i bouth st4sim-200 ic and want add more sim profiles. But dont know which tool to use for that action.

    Agostino VANORE
    ST Employee
    January 21, 2025

    Hi, the ST4SIM-200 is configured with 1GLOBAL (former Truphone) connectivity, and 1GLOBAL is also configured as Subscription Management platform (SM-SR), able to manage remotely the profile on the eSIM.

    According the GSMA SGP.02 specification/architecture, the new profile to be downloaded, shall be available on the SM-DP of the operator and the SM-DP integrated with the SM-SR managing the eSIM.

    That said, the profile download shall be managed through SM-SR and in that case referring to 1GLOBAL.

    The drawback/limitation of this architecture is that the SM-DP of the operator you want to download is not available on 1GLOBAL SM-SR.

    Visitor II
    January 21, 2025

    Understand, but cannt add custom profile of my network provider. Or can it programing by some toolkit