How to configure the STUSB4500L I2C interface without a dedicated uC/I2C Master?
Hello,
I am looking into designing a board (sink only) which uses said IC to allow me to use the 15W from the source/PD-compliant source.
From what I understand, the I2C interface attached to a master is used (in addition to other functions) to communicate what Power Delivery Output the IC should demand from the source.
Now, I want to omit having to communicate through a master. Is it possible to for example set a wanted power level via GPIOs? This way I can implement dip switches or something comparably easy to configure a specific Power Delivery Output.
I simply want to be able to make the STUSB4500L negotiate 5V at 3A from the source for me to use it elsewhere on the board.
Thanks in advance,
Michael