How to put BlueNRG2 in power saving mode with DTM app over API?
Hi everybody,
I'm using the BlueNRG M2 module on a custom hardware with a separate Host controller. It is a battery driven device so the power consumption should be as low as possible when BLE communication is not needed.
The Application Note AN4820 describes the low power modes of the BlueNRG SoC but how can i put the module into the power saving mode over the HAL API?
I can not find any API commands to control the power consumption of the BlueNRG over a host controller.
What is in general the best practise to save maximum of power without powering off the supply voltage?
Thanks a lot in advance.