Solved
This topic has been closed for replies.
Welcome, @Klim.1, to the ciommunity!
You didn't write which component you were talking about, but it's either VNH7070 or VNH7100.
The pins marked in red are clearly the outputs of the half bridges, as can also be seen in the datasheets, Fig. 15. The GND pins are in exactly the right place (pin 1, 8, 9, 16) and are connected to the sources of the low-side FETs (top and bottom die). A recommended layout is shown in Fig. 17 of the datasheet.
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.