I cant connect toBLUENRG 232 IC to BLUENRG ST link utility , Target not connected.
Pin connection:
ST link ------ BLUENRG232
SWDIO SWDIO
SWCLK SWCLK
GND GND
3.3V VCC
I have also made IO7 high with 10K resister To HIGH.
I am using IC and supporting Circuit.
I made PCB with supporting circuit for BLUENRG232 IC . The St link utility is not detecting the target.
XRCGB32M000F2P26R0Crystal, 32 MHz, SMD, 2mm x 1.6mm, 20 ppm, 5 pF, 20 ppm, XRCGB Series
used oscillator
I had followed " section 3.21 of this Datasheet reports the SWD debug feature."