i2c not working in release mode IAR
Hello,
I would to access to i2c devices with bluenrg-355MT, I use functions from BlueNRG-LP DK 1.0.0, in bluenrg_lp_evb_i2c files. When I Download and Debug, i2c works fine, but in release mode there is no i2c signals.
Here my code to detect light sensor :
BSP_I2C_Init();
HAL_StatusTypeDef ret;
ret = HAL_I2C_IsDeviceReady(&hi2cx, 0x10<<1, 1, 10);
if( ret != HAL_OK )
printf("Device not present.\r\n");
else
printf("Light sensor detected.\r\n");Whatever the parameters, there is no signals.
I2C is configured like this :
/* Initialize the GPIOs associated to the I2C port */
BSP_I2C_DATA_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
LL_GPIO_SetPinPull(BSP_I2C_DATA_GPIO_PORT, BSP_I2C_DATA_PIN, BSP_I2C_DATA_GPIO_PULL);
BSP_I2C_DATA_GPIO_AF();
BSP_I2C_CLK_GPIO_CLK_ENABLE();
LL_GPIO_SetPinMode(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetPinSpeed(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, LL_GPIO_OUTPUT_OPENDRAIN);
LL_GPIO_SetPinPull(BSP_I2C_CLK_GPIO_PORT, BSP_I2C_CLK_PIN, BSP_I2C_CLK_GPIO_PULL);
BSP_I2C_CLK_GPIO_AF();
/* Initialize the I2C clock */
BSP_I2C_CLK_ENABLE();
LL_I2C_Disable(BSP_I2C);
/* Configure the SDA setup, hold time and the SCL high, low period
* For Fast-mode 400 kHz, PRESC | 0h | SCLDEL | SDADEL | SCLH | SCLL
* 1h | 0h | 3h | 2h | 03h | 09h
*/
LL_I2C_SetTiming(BSP_I2C, 0x10320309);
/* Enable Clock stretching */
LL_I2C_EnableClockStretching(BSP_I2C);
/* Enable Peripheral in I2C mode */
LL_I2C_SetMode(BSP_I2C, LL_I2C_MODE_I2C);
/* Enable the I2C peripheral */
LL_I2C_Enable(BSP_I2C);Its I2C1 CLK-PA0 DATA-PA1
Could debug mode force peripheral to work by enabling all clocks and power paths, so i forgot to enable something ? Or what the difference between release and debug in µC configuration point of view ?
Thanks for any help,
Andy.