ICCID and Activation of ST4SIM-300M eSIM
Hi,
I’m currently working with an ST4SIM-300M eSIM and testing it for an IoT application.
I was able to read the following ICCID from the device:
89019990001234567893
I wanted to ask if anyone knows which operator or profile this ICCID belongs to. Also, I’m not sure how the activation process should work for the ST4SIM-300M.
Does it come with any initial bootstrap profile for network access, or do I need to provision a profile first before it can connect?
AT%PINGCMD=0,"8.8.8.8"
OK
AT+CPIN
ERROR
AT+CSQ
+CSQ: 99,99
OK
AT%PDNSET?
%PDNSET: 1,,IPV4V6,,,,,0,0,0
OK
at+cops?
+COPS: 0
OK
at+cops=0
At the moment I’m not able to get network connectivity, so any guidance on the correct activation/provisioning steps would be really helpful.
Thanks in advance!