Inquiry Regarding USB PD Controller Solution to use in simultaneously Charging and Data transfer on USB Upstream port.
- August 8, 2025
- 1 reply
- 1217 views
Hello,
Our product is currently in the testing phase, and we are using the USB2534 hub IC for both data transfer and device charging on downstream port.
In our setup, we are using USB 2.0 with a Type-C connector. A pen drive or mobile phone is connected to the downstream port of the USB2534, while an iPad, MacBook, or laptop is connected to the upstream port.
Data transfer on the downstream port and mobile charging are working well.
However, our key requirement is to enable iPad charging on the upstream port while the iPad is connected as a host and transferring data simultaneously.
Could you please suggest a suitable USB PD controller IC or any other solution that could meet this requirement?
A simple block diagram of our device is attached for batter understanding.
Looking forward to your guidance.
Best regards,
Tushar Raval.