Visitor II
January 4, 2026
Question
interfacing STEVAL-IOM001V1 with STSW-IOLINKGUI to get reading from SICK DT35 distance sensor.
- January 4, 2026
- 2 replies
- 502 views
Im trying to get the reading from distance sensor SICK DT35 through STEVAL-IOM001V1 which uses the L6360 IC via STSW-IOLINKGUI to get the proper reading we need to upload the IODD file of the sensor which I'm not be able to do with the GUI. There's not sufficient information about the GUI which is the cause of the problem so provide the needed documentation otherwise provide us the way to get the value from the sensor. and specify that what is the STSW-IOLINKGUI for is it just to test the connection via running the LED BLINK code.
Give me a detail documentation to understand all the functions of the GUI.