Skip to main content
JMill.18
Associate II
July 29, 2024
Question

IO-Link M12 cable for STEVAL-IDP004V2 and STEVAL-IDP003V1 connectivity

  • July 29, 2024
  • 0 replies
  • 551 views

The IO-Link Master (multiport-hub) M12 port on the STEVAL-IDP004V2, has threads on the outside and is female on the inside.

The M12 on the STEVAL-IDP003V1 has threads on the outside, and pins on the inside.  Both are 4 or 5 pin compatible.

 

I need cable with a collar on the outside at both ends to go around the threads, and on the inside, male at one end and female at the other to connect the kits.

 

I can't find an assembled cable to connect the two because cables labelled M12-male have threads on the outside and pins on the inside and the M12-female has a collar on the outside and holes on the inside.

What part number is needed to connect the two boards together? 

A 1 metre length cable would suffice.

Thank you,

-James