Skip to main content
RAlma.1
Associate II
December 6, 2023
Question

is it possible to configure LSM6DSL wake up (interrupt line) from the Linux userspcae ?

  • December 6, 2023
  • 0 replies
  • 618 views

Hi,

Thanks for your help in advance.

I have a custom Linux board with a lsm6dsl module on the platform. The driver has been ported and I can read the Accelerometer and Gyro raw data from the Linux usersapce sysfs file entries. an interrupt line from the lsm6dsl module is connected to the main processor.

I wonder if it is possible (and How) to configure to lsm6dsl module via Linux sysfs entries to generate the interrupt once the module is in certain orientation or when it detects a shock wave. image shows available sysfs entries for accelerometer and the gyroscope.

Screenshot from 2023-12-06 15-08-36.png

Many thanks,

This topic has been closed for replies.