Skip to main content
NAwari
Associate II
July 12, 2021
Question

Is it possible to switch between ASK modulation and unmodulated CW in S2LP without having to restart the Tx mode?

  • July 12, 2021
  • 0 replies
  • 551 views

I am using the S2LP Tx module for transmitting data with ASK modulation. After the end of the data, I want to transmit CW continiusoly. I see that one can change the register settings to switch between ASK and unmodulated (CW) mode. But my question is whether while switching between ASK to CW and CW to ASK, can I change the register settings without having to stop my Tx?

Is it possible to change the register settings without having to restart the operating mode of the S2LP?

best,

Nilesh

    This topic has been closed for replies.