Skip to main content
Ekko Burt
Visitor II
August 18, 2022
Question

Is there an IBIS model for the 54AC2525 with the 3.0V/3.6V MIN/MAX process corners for worst-case analysis?

  • August 18, 2022
  • 1 reply
  • 1118 views

The 54AC2525 IBIS Model does not have worst-case corners set up in the model. The model is instead set to run at TYP (3.3V), MIN (2.5V), and MAX (5V). Typically, MIN and MAX are process corners are 3.0V and 3.6V covering the min/max supply. Is there a way to get an ibis model with the actual worst-case/best-case corners at 3.3V? Thanks!

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    August 18, 2022

    This stuff would typically come via your local sales/support office, and business contacts there.

    Here, perhaps an Online Support Request directly.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..