Skip to main content
MMcDo.11
Associate
June 14, 2021
Question

Issue with receiving Ethernet data (STM32F429ZIT6 - DP83848 PHY – MII mode)

  • June 14, 2021
  • 2 replies
  • 1301 views

I am trying to get the LwIP_TCP_Echo_Client example to work on my custom board.

I never get past the HAL_ETH_GetReceivedFrame.

 /* get received frame */

 if (HAL_ETH_GetReceivedFrame(&heth) != HAL_OK)

   return NULL;

The board I am using has a STM32F429ZIT6 connected to a DP83848 PHY

The STM32429I-EVAL was used as a reference to the custom board. Different CPU pins were used due to the use of a STM32429ZI processor. Interrupt pin goes directly to the processor instead of to an expansion chip.

The hardware is connected MII.

   /**ETH GPIO Configuration

   PC1    ------> ETH_MDC

   PC2    ------> ETH_TXD2

   PC3    ------> ETH_TX_CLK

   PA0/WKUP    ------> ETH_CRS

   PA1    ------> ETH_RX_CLK

   PA2    ------> ETH_MDIO

   PA3    ------> ETH_COL

   PA7    ------> ETH_RX_DV

   PC4    ------> ETH_RXD0

   PC5    ------> ETH_RXD1

   PB0    ------> ETH_RXD2

   PB1    ------> ETH_RXD3

   PB10    ------> ETH_RX_ER

   PB11    ------> ETH_TX_EN

   PB12    ------> ETH_TXD0

   PB13    ------> ETH_TXD1

   PB8    ------> ETH_TXD3

   */

   /**ETH Interrupt GPIO Configuration

   PB14    ------> ETH_INT (GPIO_EXTI14)

   /**Switch GPIO Configuration

   PE6    ------> Switch_INT (GPIO_EXTI6)

Compiler:

STM32CubeIDE Version 1.6.1 build 9958_20210326_1446 (UTC)

STM32CubeMX Version: 6.2.1-RC2 Build: 20210324-1236 (UTC)

LwIP Version 2.1.2

The PHY Chip defaulted to address 1. I changed it to address 3. I read online that there might be a problem with using address 1. Neither address worked. I just changed the address via software I did not re-strap the pins.

I have been able to connect to the PHY chip and the following is a data dump of the settings:

low_level_init

PHY_PHYIDR1 : 0x2000

PHY_PHYIDR2 : 0x5c90

PHY_ANAR   : 0x01e1

PHY_ANLPAR : 0x45e1

PHY_ANLPARNP: 0x45e1

PHY_ANNPTR : 0x2801

PHY_MICR   : 0x0000

PHY_FCSCR  : 0x0000

PHY_RECR   : 0x0000

PHY_PCSR   : 0x0100

PHY_RBR    : 0x0001

PHY_LEDCR  : 0x0000

PHY_BTSERIAL: 0x0804

PHY_CDCCTRL1: 0x0000

PHY_EDCR   : 0x6011

PHY_ANER   : 0x0005

PHY_PHYCR  : 0x8023

PHY_BMCR   : 0x2100

PHY_BMSR   : 0x784d

PHY_STS    : 0x0605

PHY_MICR   : 0x0003

PHY_MISR   : 0x0020

When I press the switch to start the TCP transmission, I do not get past the ARP.

WireShark Results example:

60 ARP announcement for 10.100.0.20

60 Who has 10.100.0.23? Tell 10.100.0.20

42 10.100.0.23 is at 50:3f:56:02:5c:2c

60 Who has 10.100.0.23? Tell 10.100.0.20

42 10.100.0.23 is at 50:3f:56:02:5c:2c

I have converted the example code to STM32CubeIDE and ran it on the STM32429I-EVAL successfully.

On an O-scope, I was able to see signals on the RX_DV line and the RXD0 line. I think the data is getting through the PHY.

Has anyone experienced a problem similar to this?

Any Ideas would be greatly appreciated.

    This topic has been closed for replies.

    2 replies

    MMcDo.11
    MMcDo.11Author
    Associate
    June 15, 2021

    0693W00000Bb4iAQAR.jpg0693W00000Bb4i5QAB.jpgI wanted to add the Ethernet Portion of the schematic.

    Also the Wireshark Image.

    0693W00000Bb4ioQAB.jpg 

    MMcDo.11
    MMcDo.11Author
    Associate
    June 16, 2021

    I found a solution to my problem.

    R98 which is connected to the MII_RXD3 line was a 4.7K Resistor not a 33 ohm resistor.

    After changing that resister to a 33 Ohm the Ethernet started communicating.

    Thanks for looking at this issue.