Skip to main content
Visitor II
July 9, 2025
Question

L9663 read init data

  • July 9, 2025
  • 0 replies
  • 183 views

Hi:

    The sensor is set to 20 bits of payload, 3 bits of frame control, 1 bit of status, and 16 bits of data. Currently, the InitiatDATA-RDY bit of L9663 has been set. I use the format of initializing data to set initobuf_id to 0 and register to 1. The data sent to 9663 through SPI always returns 0x44000001. No matter what the initobuf_id and register are set to, they are all 0x44000001. I would like to ask where the error occurred。

li_he_0-1752044781152.png