L9663 Sync Pulse Interval
Dear,
From the datasheet of L9663, the minimum interval of sync pulse period is 200us. But I want to send the sync pulses with period less than 200us, how can I do it?
In the datasheet, it mentioned "If full flexibility for the sync pulse interval is required, use direct triggering either via SPI or direct interface."
But in the SPT register, it described the 200us "Minimum allowed period (if SYNC pulse trigger is generated by PIN or SPI)." The two sentences looks contradictious, or to say there is a special way to send the "direct triggering" signal?
And the 200us determined by the bootstrap circuit, but this bootstrap circuit could be bypassed. So it's possible to send the sync pulse with period less than 200us in principle.
Thank you.