Skip to main content
JAlex2
Associate
September 25, 2023
Question

LNB Efficiency

  • September 25, 2023
  • 1 reply
  • 898 views

Using the STEVAL-LNBH06 I am not able to achieve 93% efficiency as stated in the data sheet. Please advise why this might be.

inout voltage: 12V

load: 43ohm power resistor for each channel (draw 420mA per channel)

measured input power: 20.4W

output power: 17.2W

efficiency: 85%

This topic has been closed for replies.

1 reply

Issamos
Lead III
September 25, 2023

Hello @JAlex2

The 93% efficiency is for specific conditions that you can find them in the part 8 of the DS8975.

Best regards.

II

JAlex2
JAlex2Author
Associate
September 26, 2023

Are you referring to where it specifies Iout as 500mA? If so, I have already tried this condition on the evaluation board even with low power mode active, and only improved to 87%. Please advise what condition you are referring to if this is not it.