Skip to main content
TSour.2
Associate
February 22, 2023
Solved

LNBH26 works with DISEQC 22KHz, is it possible to work with LNB and diseqc on frequency 1MHz ?

  • February 22, 2023
  • 1 reply
  • 1184 views

..

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    No, according to the DiSEqC standard, only the frequency of 22kHz is supported.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards,

    /Peter

    1 reply

    Peter BENSCH
    Technical Moderator
    February 22, 2023

    Welcome, @Community member​, to the community!

    You certainly know what the 22kHz is used for with DiSEqC.

    Where then do you see the requirement for 1MHz?

    Regards

    /Peter

    TSour.2
    TSour.2Author
    Associate
    February 22, 2023

    Hello Sir,

    Thank you for your answer.

    I know that the DiSEqC protocol uses the 22 kHz signal to send its information frames, and to tell the LNB to switch between low and high band. My question is: is it possible to send the data to the LNB with a signal other than the DISEQC ?

    Thank you again,

    Peter BENSCH
    Peter BENSCHBest answer
    Technical Moderator
    February 22, 2023

    No, according to the DiSEqC standard, only the frequency of 22kHz is supported.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards,

    /Peter