Skip to main content
SBukh.1
Associate II
May 12, 2020
Question

Method for UART receive data in provided UART DTM project in BlueNRG SDK

  • May 12, 2020
  • 0 replies
  • 521 views

Using the DTM UART project "BlueNRG-1_2 DK 3.1.0/Project/BLE_Examples/DTM" there is a method to send data (transport_layer_send_data) available. However, the corresponding transport_layer_receive_data logic is blocked out by #ifdef and appears to only be available if using SPI as the communication method.

Is anyone familiar with what logic the UART DTM uses to receive data over UART?

0693W000000XITMQA4.png0693W000000XITHQA4.png

This topic has been closed for replies.