Not able to read RSSI value between two bluenrg bluetooth unit
Hi,
To measure distance between two bluenrg module using rssi value.
The two devices are loaded with BLE_Beacon example with different public address and few scanning functions are included.
Both the device advertising data can be seen in ST Ble APP in the mobile.
But at the device side,to scan and read the rssi value,the "hci_le_advertising_report_event()" event function is not invoked during scanning.
Advertising is working ,but scanning is not work at device side.
Board:STEVAL-BCN002V1B - (BlueTile)
Thanks in advance.