Skip to main content
Visitor II
September 26, 2025
Solved

QoS configuration on ST67W

  • September 26, 2025
  • 2 replies
  • 623 views

Hi, i have bought a Nucleo-U575ZI-Q coupled with a X-Nucleo-67W61M1

i have upload the exemple ST67W6X_MQTT, after reading the doc i have complete the configuration and i run well. 

I use it with mosquitto or nanomq brokers (same results) but on both the broker inform me than the QoS=0 (with publish and subscribe)

The documentation of the AT-command of ST67W indicate that i can use 0,1 or 2 for the Qos. In the exemple the drivers don't use the Qos and force it to zero. I have modify it but the result is always the same. I would like to use QoS=1 to be sure the message arrived. Have you an idea ?

I have verify than the broker accept all levels in the conf. I have also publish with MQTTX(with Qos=1) and the broker notify the good level of Qos

Best answer by TarikAb

Hi XP_LGE,

Could you test with X-CUBE version 1.2.0? It includes a fix related to QoS flags.

Best regards

2 replies

Technical Moderator
October 9, 2025

Hi XP_LGE,

 

Can you please test again with ST67W6X_MQTT project from latest release 1.1.0? QoS has been added into the application's configuration options (see ST67W611M1 Wi-Fi® – MQTT Demonstrations - stm32mcu).

Best regards,

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TarikAbBest answer
Technical Moderator
January 6, 2026

Hi XP_LGE,

Could you test with X-CUBE version 1.2.0? It includes a fix related to QoS flags.

Best regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.