Skip to main content
Associate
July 24, 2024
Question

Question about using DCMI in extra ADC(AD7768)

  • July 24, 2024
  • 0 replies
  • 722 views

我尝试使用 STM32L4R9 与 AD7768 通信,使用 8 个通道。我想知道的是:是否可以使用 DCMI 建立 AD7768 与微控制器之间的通信(微控制器支持,但我不确定 AD7768 是否支持 DCMI。)如果 AD7768 也支持,我想知道 PCB 应该如何正确布线。

Translation to English

I am trying to communicate with the AD7768 using the STM32L4R9, using 8 channels. What I want to know is: is it possible to use DCMI to establish communication between the AD7768 and the microcontroller (the microcontroller supports it, but I'm not sure if the AD7768 supports DCMI.) If the AD7768 supports it as well, I would like to know how the PCB should be wired correctly.