Visitor II
July 27, 2021
Question
S2-LP basic settings and transmitting process.
- July 27, 2021
- 0 replies
- 601 views
Hi, I have two S2- LP modul ( Radiocontrolli ) and I would like to test these but I can't start the communication. I use Microchip microcontrollers, the SPI communication is working, TX command OK, I get the nIRQ on GPIO1 ( TX data sent ) , and get back to Ready mode with SABORT command, but it seems the Receiver no response?! I don't know exactly what is the good way for transmitting?! Before TX command I set PCKTLEN0 as well and I load the data to 0xFF Register. I attached the setting file. I use these settings at both side ( TX, RX ).