Skip to main content
lukasz2
Associate III
February 10, 2021
Question

S2-LP CSMA feature in transceiver mode

  • February 10, 2021
  • 0 replies
  • 539 views

Hi,

I am trying to implement CSMA feature on S2-LP. I am working with SDK_Csma_X examples.

The SDK_Csma_A example is a transmiter and the SDK_Csma_B is receiver. I have to have the transceiver. When I combine the two examples there is no acnowledgement IRQ_TX_DATA_SENT and the second node does not receive the data. I tried to enable CSMA just before send a TX command and disable it after receive IRQ_TX_DATA_SENT in status. I also tried to switch S2-LP to ready state before enable CSMA with no result. Is there the clear guidance how to implement CSMA feature when RX mode is necessary all the time but sometimes the device have to respond by transmitting data ?

Best Regards

This topic has been closed for replies.