Skip to main content
allard
Senior
January 11, 2019
Question

S2LP: Set datarate to 500 kbps

  • January 11, 2019
  • 7 replies
  • 1408 views

According to the datasheet the S2-LP supports datarates up to 500kpbs in 4GFSK mode. In the S2-LP DK gui I can only set it to 250kpbs, what am i doing wrong?

This topic has been closed for replies.

7 replies

lgrz
Visitor II
April 10, 2020

Have the same problem. Setting the 500kbps and 4(G)FSK modulations in bare-metal example makes that two S2LP based boards (STEVAL-FKI868v2) do not see each other packets. Trying to set these parameters in S2-LP DK GUI does not work - as @allard mentioned it is not possible to set data rate higher than 250kbps. Entering any value greater than 250kbps, the GUI automatically limits to 250. Has anybody know what is the cause and the possible solution ? Many thanks for any advice.

VClar.1
Visitor II
April 30, 2020

Did either of you, Igrz or allard, get 4gfsk to work at high data rates, >=100kbps, with low BERs?

lgrz
Visitor II
April 30, 2020

Hi @VClar.1​, unfortunately I couldn't achieve satisfying BER results with 4GFSK and more than 100kbps (76.8 kbps was the max), while higher DR (up to 250kbps) and low BER was affordable with 2FSK only.

VClar.1
Visitor II
May 11, 2020

@lgrz​ Thanks for the reply!

PPelg.1
Associate
June 26, 2021

Dear, where can I find required settings for S2-LP to archief 250kbps or 500kbps ?

What should be the frequency deviation and channel frequency filter for different modulation types ?

is there somewhere an STM document explaining data rate, frequency deviation and frequency filter settings ?

Greetings,

Patrick

Winfred LU
ST Employee
June 29, 2021

Please consider the column data rate as symbol rate.

In 4GFSK each symbol has 2 bits, so to obtain 500kbps data rate you have to set the symbol rate 250ksps.