RShiv.1Associate IIIForum|Forum|3 years agoNovember 15, 2022Questionsensor when connected using I2C to ST25R3911B we are seeing any activityForum|Forum|3 years agoNovember 15, 20222 replies1521 viewsHi,attached is the code for I2C where we are trying to read from the sensor connected using I2C...I2C_mem_write or I2C_Master Transmit...nothing is sent by the sensor.any change in the coonfiguration ..kindly let us know.attached the IOC file also...Thanks and regardsRavi chandranmain.cDisco_UART_I2C.iocI2CUART-USART