Sometimes I'm reading strange values for RMS voltage and current on my STPM32, but I do not know why. Is there something very special to concider?
Hello,
I'm using a STPM32 to measure the ac line voltage and current. It is connected via a galvanic isolator ISO7341CDW to a STM32F072 with SPI. Most of the time, this works just fine. I can read the correct RMS values for I1 and V1 (Register DSP_REG14 at 0x48) as well as the period (Register DSP_REG1 at 0x2E) to convert it to the line frequency. I can change the ac voltage with a adjustable transformer and see the correct values. I'm polling the values every 1 second, but the STPM32 is set to autolatching.
So sometimes something seem to go wrong:
- Sometimes I get the correct voltage value but a strange value for the current. Starting from a value of ~3000 mA it decreases to zero and then again starts at ~3000 mA etc. When I change the ac input voltage, still the correct voltage value is read by the STPM32, but the current value stays wrong. When the ac voltage is decreased to ~85 VAC, the current decreases to 0 and stays there, even when the ac input voltage is increased again.
- Sometimes I get the correct current value but a strange value for the voltage. Starting from a value of 400 VAC it decreases to zero and stays there forever, no matter what the input voltage will be changed to after that.
- Sometimes both the voltage and current values are strange. So both values show the behavior described above.
- The measurement of the period (register DSP_REG1) works just fine all the time, even when the voltage or current values are strange.
I just read some of the received data from register DSP_REG14 in the Atollic True Studio for debugging purposes. These data frames were received exactly in this order with no other frame in between after flashing and starting the firmware to the STM32F072 in debug mode. The actual ac voltage was ~130 VAC, the actual current was ~240 mA.
1) rx_data[0] 0x13 (V1 RMS Data [7:0])
rx_data[1] 0xda (V1 RMS Data [14:8], C1 RMS Data [15])
rx_data[2] 0x7f (C1 RMS Data [23:16])
rx_data[3] 0x03 (C1 RMS Data [31:24])
rx_data[4] 0x9d (CRC)
VOLTAGE_RMS 461.180 VAC (calculated)
CURRENT_RMS 234 mA (calculated)
2) rx_data[0] 0xc4 (V1 RMS Data [7:0])
rx_data[1] 0x18 (V1 RMS Data [14:8], C1 RMS Data [15])
rx_data[2] 0x82 (C1 RMS Data [23:16])
rx_data[3] 0x03 (C1 RMS Data [31:24])
rx_data[4] 0x94 (CRC)
VOLTAGE_RMS 126.800 VAC (calculated)
CURRENT_RMS 234 mA (calculated)
3) rx_data[0] 0x12 (V1 RMS Data [7:0])
rx_data[1] 0x16 (V1 RMS Data [14:8], C1 RMS Data [15])
rx_data[2] 0x81 (C1 RMS Data [23:16])
rx_data[3] 0x03 (C1 RMS Data [31:24])
rx_data[4] 0x3e (CRC)
VOLTAGE_RMS 113.000 VAC (calculated)
CURRENT_RMS 234 mA (calculated)
4) rx_data[0] 0x00 (V1 RMS Data [7:0])
rx_data[1] 0x00 (V1 RMS Data [14:8], C1 RMS Data [15])
rx_data[2] 0x80 (C1 RMS Data [23:16])
rx_data[3] 0x03 (C1 RMS Data [31:24])
rx_data[4] 0xbf (CRC)
VOLTAGE_RMS 0 VAC (calculated)
CURRENT_RMS 234 mA (calculated)
5) rx_data[0] 0x00 (V1 RMS Data [7:0])
rx_data[1] 0x80 (V1 RMS Data [14:8], C1 RMS Data [15])
rx_data[2] 0x82 (C1 RMS Data [23:16])
rx_data[3] 0x03 (C1 RMS Data [31:24])
rx_data[4] 0x9e (CRC)
VOLTAGE_RMS 0 VAC (calculated)
CURRENT_RMS 235 mA (calculated)
I first thought about corrupted data packages, but it seems like the CRC is right. Also, when the ac input voltage is read wrong, the current value is still perfectly correct. Even Bit 15 of register DSP_REG14 fits to the current value. This Bit represents the LSB of the current value.
I also do not think, that it is a problem due to wrong calculation in the STM32F072 e.g. overflow, as it works most of the time just fine in the full range of ~80 VAC to 270 VAC. Also I'm using uint32_t values there and verified this independently.
In the STM32F072 I'm using this command to receive the data shown above. Is this fine or would be the single command "HAL_SPI_TransmitReceive(&hspi2, tx_data, rx_data, 5, 1000);" be better?
//////// prepare array for reading data
// - first Byte = Address to read = 0x48 = DSP_REG14
// - Byte 2-4 = could be command to write, but will be ignored when set to 0xFF
// - Byte 5 = CRC, calculated by separate function. Set to 0x99 for debugging
uint8_t tx_data[5] = {0x48, 0xFF, 0xFF, 0xFF, 0x99};
// reset CS-signal for sending the read request
HAL_GPIO_WritePin(NSS_GPIO_Port, NSS_Pin, GPIO_PIN_RESET);
// send and receive request data via SPI
HAL_SPI_Transmit(&hspi2, (uint8_t*) tx_data, 5, 1000) );
// set CS-signal
HAL_GPIO_WritePin(NSS_GPIO_Port, NSS_Pin, GPIO_PIN_SET);
HAL_Delay(1);
// reset CS-signal for receiving requested data
HAL_GPIO_WritePin(NSS_GPIO_Port, NSS_Pin, GPIO_PIN_RESET);
// receive data via SPI
HAL_SPI_Receive(&hspi2, (uint8_t *) rx_data, 5, 1000);
// set CS-signal
HAL_GPIO_WritePin(NSS_GPIO_Port, NSS_Pin, GPIO_PIN_SET);Has anyone any idea, what this problem could be about?