ST eSIM doubts (profile, pre-programming)
Hi.
Currently we use SIM7000G and SIM7070G (GSM, NB-IoT, LTE-M, GNSS) modules from Simcom in our projects, using for authentication only a SIM holder with plastic chip, in the old way. We are starting to integrate the eSIM ICs on the boards, to use holder for plastic SIM + eSIM IC + dual SIM card analog MUX, I already did a layout including these 3 things, but still have doubts about the the eSIM.
I have sent this email do Simcom support:
"Hi, we would like to know if, for SIM7000G and SIM7070G modules, if they are compatible and can work with eSIM chip/IC like the ST4SI2M0020TPIFW of ST Microelectronics, we plan to use this one. Do I just need to connect the electronic signals of the SIM interface of the modules to the same named signals of the eSIM chip/IC?
I saw that in Brazil, for the newer smartphones integrating an eSIM, the network operator would generate a QR code to the user, who would scan it with the camera and then the smartphone would write informations in the eSIM chip. But how the same operation would work for IoT devices which uses Simcom modules? Will the modules maybe require firmware update to become compatible?
Can you give us a guide? The Simcom modules in question are the SIM7000G and SIM7070G."
Their answer was:
"Yes, the SIM7000G and SIM7070G modules are compatible with eSIMs of any brand.
When purchasing the chips, you will have to contact the manufacturer and provide the profile that you want to be installed on this eSIM. No modification to the modules firmware is required."
Then I sent back a second email:
"May I ask 2 question?
(1) In eSIM chip/IC, is there the need to write/program something on it before soldering it to the board/PCB? I mean a write/program done directly in the hardware, directly on the pins of the IC, using a specific tool to make this function.
(2) If the module (SIM7000G ou SIM7070G) be supplied, and having the cellular antenna and eSIM connected to it, is this sufficient to be able to install/write the profile in the eSIM through the cellular network?"
But they did not replied this second email. About question (1) and (2) above, could somebody from ST help me? These are doubts I have and searched a lot on internet and didn't found the answer.
How is the procedure to contact the eSIM manufacturer to install the profile?
Please, I would like a clarify about these questions.
Regards,
Jeferson.