ST67W611M1 wrong data received through SPI
Dear all,
I'm trying to control ST67W611M1 wifi module by using a linux host chip. After flashing the newest firmware I reset the module to SPI mode. Some logs can be received through the uart interface and the SPY_RDY pin is drived to high level. But I just receive 0xAA 0x55 0x09 through SPI, it seems not a 'Ready' signal.
I am sure that the SPI is configured as requested, which is confirmed by using a oscilloscope. What should I do to solve this problem? Besides, That would be great if a linux-based SDK can be provided.
Thanks