Skip to main content
EBono
Visitor II
May 12, 2020
Question

STEVAL-BLUEMIC-1signal strenght

  • May 12, 2020
  • 0 replies
  • 403 views

We are working with 2 STEVAL-BLUEMIC-1 boards, one configured as server and one configured as client. Server is located into a PVC box at about 2/3 meters from the client. We noticed that when we hold in hand the pvc box or when we interpose ourselves between the 2 boards we lose communication (disconnection event is generated). We already did some tests and we think that the problem could be the strenght of the signal. On both software we set "aci_hal_set_tx_power_level(1;7);" so the power level shoul be the maximum. We would like to know if it's possible to increment the signal strenght in some way, maybe using a more powerful antenna. The clien is directly connected to a power source, so on that side we don't care about energy saving. Have you got any suggestion on how we could increment signal strenght?

Thanks

This topic has been closed for replies.