STEVAL-IDB008V1M (BlueNRG-2 SoC) does not establish VCP port on PC, only STM DFU
Since the poorly soldered microUSB connector on the eval board broke off, I fixed and wired USB-A connector. If the board is then connected to PC, STM DFU device appears in Device Manager and appropriate driver could be installed so I suppose that the wiring is O.K. However, originally a USB Serial Port (COMx) appeared so either the RF-Flasher Utility or a terminal program can work with the board.
What could be the cause of this?