STM BlueNRG-MS Max Characteristic length limited to 255 due to aci_gatt_add_char function limitations.
My general understanding is that the BLE standard supports characteristics with a lenght of up to 512 bytes. I'm using the BlueNRG-MS chip from STM but there the function call to add a characteristic has a uint8_t value for the length parameter
tBleStatus aci_gatt_add_char(uint16_t serviceHandle,
uint8_t charUuidType,
const uint8_t* charUuid,
uint8_t charValueLen,
uint8_t charProperties,
uint8_t secPermissions,
uint8_t gattEvtMask,
uint8_t encryKeySize,
uint8_t isVariable,
uint16_t* charHandle);
So this would allow only a maximum characteristic length of 255 bytes. According to this document the stack itself supports 2 bytes with FW 7.2 or higher. I have 7.23 so this should be fine but I cannot find any reference or example of a BlueNRG-MS middleware that would support a call with
charValueLen
of type
uint16_t
. I also downloaded the latest STSW-BLUENRG-DK and the examples also only support
uint8_t charValueLen
.