Skip to main content
Associate
April 30, 2024
Solved

STPM33/34 MISO & Insulating barrier

  • April 30, 2024
  • 11 replies
  • 3449 views

Hello everyone

I am looking into the STPM33/34. I only want to use 1 SPI bus for both ICs and select it with the SCS.

In the datasheet I cannot see whether the MISO goes into tristate when the IC in question is not active.

I also cannot see any information about the galvanic isolation/barrier.

Can anyone give me information about this.
Thank you in advance.

Best answer by AScha.3

Hi,

>I also cannot see any information about the galvanic isolation/barrier.

Right, because there is no isolation/barrier .

11 replies

Didier HERROUIN
Technical Moderator
June 14, 2024

Hello,

The MISO line is in Hi-Z mode when the STPM3x is not selected (SCS at high level).

Just note this limitation in case you use several STPM3x in parallel: 
https://www.st.com/resource/en/errata_sheet/es0591-stpm3x-device-limitations--stmicroelectronics.pdf

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.