STPM33/34 RMS Current Calculation Error
Hi everyone,
I met a problem when I measured the current rms value with stpm33 ic.I'm using this IC with resistive loads and other load profiles with low crest factor. But I met a case with a high crest factor load like as SMPS type loads.
I collected the momentary current datas from STPM33eval board over SPI lines. And than calculate the RMS current value using with point by point datas. The calculated value asme as real value. I compared the calculated value with true RMS values that are measured with other power analyzers as called as Vitrek PA900 and Schneider PA module.
I compared the current values with resistive and refrigerature type loads. They are same for all measurement device.
Is it possible to make any mistake when I config the STPM?
You can find my measured values and voltage-current graph at below.
Blue: Actual Voltage Orange: Actual Current
| Load | STPM33 Current RMS(mA) | STPM33 Current Calculated RMS(mA) | Vitrek PA900 RMS(mA) | Scheneider PM2200 RMS(mA) |
| High Crest Factor SMPS Load | 119,9 | 199 | 198 | 198 |
| Low Crest Factor Load (Resistive Load) | 1033 | 1033 | 1033 | 1033 |