Skip to main content
Gjain.1
Associate II
October 27, 2021
Solved

STUSB1700 For current 1.5A to 3A variation or lesser , can we still use 3.0A USB type C current source capability? OR Can we defining Rp_def logic level as 1 and Rp_HIgh also 1 for variable current from 500 mA to 3A? Thanks

  • October 27, 2021
  • 1 reply
  • 584 views

0693W00000FDrRLQA1.png

    This topic has been closed for replies.
    Best answer by Winfred LU

    Yes, as it defines the source current capability. The actual current depends on the device being attached.

    1 reply

    Winfred LU
    Winfred LUBest answer
    ST Employee
    October 29, 2021

    Yes, as it defines the source current capability. The actual current depends on the device being attached.