[STUSB4500] Can I remove the typical circuit on STUSB4500's VBUS_VS_Disch pin?
Hello,
In the STUSB4500 datasheet, there are 2 typical circuits. Both of them include a circuit for the VBUS_VS_Disch pin. Components are D4, C4, R1 and R4. Based on the information in the datasheet, this circuit should be here to limit the discharge current to 50mA. Moreover, this pin is used by the chip to sense vbus voltage.
What's the purpose of the diode D4?
Discharge feature is optional and can be disabled in NVM. I want to disable it in my application, do I still need to link VBUS_VS_Disch to VBUS to sense VBUS? If so, what is the minimal circuit, do I need some resistors?
Thanks,
Arthur