STUSB4500, can the GPIO (or attach) pin be used to control a MOSTFET for a different power path
Hey ST
I am building an application that has two power sources, one USB-C (27W) with the STUSB4500 controller, and an optional DC input.
Because the GPIO or attach pins can be open drain, theoretically they could be used to contrl a second FET on the power path of the DC input. Do you guys think the STUSB4500 could handle this?
Also, because the two inputs would be joined, to block revers current, would the STUSB4500 support a back to back FET configuration for the SNK MOSTFET?
The power supply's do not need to be uninterruptible, so switching time is not an issue.
The two power souses will not be present at the same time.
Blue - current path when USB-C cable is plugged in, and sourcing power
Red - current path of DC connector, no USB-C plug present
The on board MCU will use I2C to comunicate with the 4500, if the attach pin could be used to switch the power path of the DC input, that should make is so when a usbc cable is plugged in, the DC input is disabled
Thanks
Jonas