Skip to main content
ABouk.1
Associate III
May 4, 2021
Question

Teseo liv3F uses 3 satellites but does not get a position

  • May 4, 2021
  • 2 replies
  • 1036 views

Good morning,

I have been struggling with a custom board that contains the Teseo liv3F. When debugging the module with Teseo suite pro, i can see good signal levels from 3 GPS satellites but the Fix Mode is set to NO FIX and the Lat = Long = 0.

How can I get a valid position from 3 sats ?

This topic has been closed for replies.

2 replies

DN_1
Associate II
May 31, 2021

Hi there,

I have also started recently working with the Teseo and have encountered this behaviour when I trigger a cold start.

Alternatively I found a setting on in the software manual "CDB-ID 222 – LMS operating mode setting 1" where it looks like you can disable a 2D fix on the Teseo, which would mean that it probably requires 4 satellites at least to get a fix.

Tesla DeLorean
Guru
May 31, 2021

Get a better antenna/location, the signal strength is woeful, you won't be able to pull navigation data (ephemeris) at those levels. The alternative would be to get that data via a network, ie AGPS

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..