Skip to main content
Anitha
Associate III
May 14, 2020
Question

user error: reset failed in IAR while and download the debug the lightning_demo project to STEVAL-IDB008V2 in IAR

  • May 14, 2020
  • 0 replies
  • 641 views

I'm using the IAR(8.40.1) for flashing the code(Lightning_demo from stsw-bnrg-mesh package) using stlink. After pressing the download and debug icon i'm facing User error: Reset failed.

But while flashing with BlueNRG1 ST-Link Utility, I was able to flash the code success fully.

At the same time if press on the debug without downloading then i was seeing fatal error: ST-Link, No MCU device found. Could u please help me to resolve the issue.0693W000001cGEiQAM.png0693W000001cGDVQA2.png

0693W000001cGB6QAM.png

This topic has been closed for replies.