Using BlueNRG-LP as BlueNRG-2
Hello everyone,
I recently successfully used a BlueNRG-2 chip for a BLE project (connected to an external microcontroller and integrating the BlueNRG-2 API by means of .ioc project manager). However, it needed a very small baloon which has been a real mess to solder by hand. I then saw that the BlueNRG-LP comes with the baloon integrated, which could help me hand-soldering the PCBs.
However, the BlueNRG-LP doesn't come with a preflashed image. Is there any available image by ST that I can flash on the BlueNRG-LP that will let me keep using the same (or at least similar) APIs used on the BlueNRG-2? I think that including the libraries via STM32CubeIDE Project Manager really speeds up the programming time.
Thank you for reading,
Mariano